Execution code in ram

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Execution code in ram

2,670件の閲覧回数
markulhu
Contributor II

hi, for my eeprom driver designing, i copyed the code from flash to ram,but jump to code in ram, it cause "HardFault" exception. is there any configuration that must be set manually? 

//static Std_ReturnType Eep_EnEepRam(void)

{

FTFC_FCCOB0 = 0x81; /* SETRAM */
FTFC_FCCOB1 = 0x00; /* FlexRAM available for emulated EEPROM */
FTFC_FSTAT |= 0x80; /* Launch command */
while (FTFC_FSTAT & 0x80) {}
return FTFC_FSTAT == 0? E_OK: E_NOT_OK;

}

//void Eep_Init(void)

{

const uint8* EnEepFun;
uint8* LoadRam = (void*)0x1FFFF000;
uint32 Depart;

Depart = (SIM_FCFG1 & 0xF000) >> 12;


if (Depart == 3 || Depart == 4 || Depart == 8 || Depart == 10 || Depart == 11)
{
EepRamEnabled = TRUE;
return;
}

EnEepFun = (const void*)Eep_EnEepRam;

(void)memcpy(LoadRam, EnEepFun, 20);
if (((Std_ReturnType(*)(void))LoadRam)() == STD_OK)
{
EepRamEnabled = TRUE;
return;
}

}

2 返答(返信)

2,585件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Steven,

You can use code below to place the function into the RAM and after that just use the name of the function to call.

__attribute__ ((section(".code_ram"))) // place the code below into .code_ram section
void YourFunction(void);

Or you can check the S32_SBC[CFSR] register. For more details, please, look at the Cortex-M4 Devices Generic User Guide, chapter 4.3.10: http://infocenter.arm.com/help/topic/com.arm.doc.dui0553b/DUI0553.pdf  

I assume that you use S32K14x.

I hope it helps.

Best regards,

Diana

0 件の賞賛
返信

2,585件の閲覧回数
markulhu
Contributor II

Diana,thanks for your advice!  i have located the reason ,that  because the lowest bit of PC of thumb code must be 1. so i changed LoadRam's value from 0x1FFFF000 to 0x1FFFF001,  it seems running ok.

thank you for your help again!