Examples for EBT plugins for S32K144

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Examples for EBT plugins for S32K144

ソリューションへジャンプ
3,009件の閲覧回数
yash_bhatnagar9
Contributor II

Hi, I am looking for the example for EBT plugins, to test out the configuration. I have the same for S32K3 board but not for the S32K144 board. I have attached an image for the folder structure for S32K3 RTD. I am looking for the same for S32K144 board if available.

タグ(1)
0 件の賞賛
返信
1 解決策
2,990件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Unfortunately, the example for each modules as for K3 is not available for K1 yet. With S32K1xx AUTOSAR MCAL products, we have either the sample application located in each package (e.g. S32K14X_MCAL4_2_RTM_1_0_1\S32K14X_MCAL4_2_RTM_1_0_1_Sample_Application), or the platform integration which should be available here: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K1XX-PTFM01D 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,991件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Unfortunately, the example for each modules as for K3 is not available for K1 yet. With S32K1xx AUTOSAR MCAL products, we have either the sample application located in each package (e.g. S32K14X_MCAL4_2_RTM_1_0_1\S32K14X_MCAL4_2_RTM_1_0_1_Sample_Application), or the platform integration which should be available here: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K1XX-PTFM01D 

0 件の賞賛
返信