Examples for EBT plugins for S32K144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Examples for EBT plugins for S32K144

Jump to solution
2,998 Views
yash_bhatnagar9
Contributor II

Hi, I am looking for the example for EBT plugins, to test out the configuration. I have the same for S32K3 board but not for the S32K144 board. I have attached an image for the folder structure for S32K3 RTD. I am looking for the same for S32K144 board if available.

Tags (1)
0 Kudos
Reply
1 Solution
2,979 Views
namnguyenviet
NXP Employee
NXP Employee

Unfortunately, the example for each modules as for K3 is not available for K1 yet. With S32K1xx AUTOSAR MCAL products, we have either the sample application located in each package (e.g. S32K14X_MCAL4_2_RTM_1_0_1\S32K14X_MCAL4_2_RTM_1_0_1_Sample_Application), or the platform integration which should be available here: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K1XX-PTFM01D 

View solution in original post

0 Kudos
Reply
1 Reply
2,980 Views
namnguyenviet
NXP Employee
NXP Employee

Unfortunately, the example for each modules as for K3 is not available for K1 yet. With S32K1xx AUTOSAR MCAL products, we have either the sample application located in each package (e.g. S32K14X_MCAL4_2_RTM_1_0_1\S32K14X_MCAL4_2_RTM_1_0_1_Sample_Application), or the platform integration which should be available here: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K1XX-PTFM01D 

0 Kudos
Reply