Error occurred while connecting to the interface hardware or target

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Error occurred while connecting to the interface hardware or target

跳至解决方案
3,879 次查看
Anilpatil_SasvaAuto
Contributor IV

Hello Team,

I am using S32K144EVB and tried to run a sample application(hello_world_s32k118) with PE micro debugger (built-in OpenSDA) to check if the EVB is fine. Things were not going well and got errors as below.

Anilpatil_SasvaAuto_0-1715345747182.png

Anilpatil_SasvaAuto_1-1715345758763.png

Please provide the solution ASAP

0 项奖励
回复
1 解答
3,774 次查看
Anilpatil_SasvaAuto
Contributor IV
It is working now, the issue is with the power supply. need to change J107 for USB supply
Thanks for the support.

在原帖中查看解决方案

7 回复数
3,786 次查看
Anilpatil_SasvaAuto
Contributor IV

Hello World code

0 项奖励
回复
3,776 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Have you already referred to that link?
Please tell me which step does not meet expectations.
If you don't tell me in detail, I won't be able to help you solve this problem.

0 项奖励
回复
3,775 次查看
Anilpatil_SasvaAuto
Contributor IV
It is working now, the issue is with the power supply. need to change J107 for USB supply
Thanks for the support.
3,854 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Since you are using S32K144EVB, why do you want to run a sample application(hello_world_s32k118)? Please run the S32K144 example in the future.

I happened to be discussing a similar issue with another customer, please refer to: S32K144 EVB Red led 계속 on 상태입니다.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
3,559 次查看
Anilpatil_SasvaAuto
Contributor IV
 
0 项奖励
回复
3,846 次查看
Anilpatil_SasvaAuto
Contributor IV

Sorry, it's a copy mistake. I have run the S32K144 example.

Anilpatil_SasvaAuto_0-1715577432997.png

 

0 项奖励
回复
3,840 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Which example codes do you loaded into the device? Any for CSEc?
Did you secure the device?(FSEC SEC=secured )

Doesn't P&E Recovery Utility halt MCU? Please tell me what problem occurred during the operation.

0 项奖励
回复