Error in S32K358 Memory Stack Configuration: Missing "Fee_SetMode" Function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error in S32K358 Memory Stack Configuration: Missing "Fee_SetMode" Function

1,699件の閲覧回数
Ahmed_Huzien
Contributor I

Hello,

I'm currently working on configuring the memory stack for the S32K358 target. I am using the NXP MCAL package, specifically the Mem_43_InFls, MemAcc, and Fee modules. Additionally, I'm utilizing the Vector Package for the Basic Software (BSW) components, including MemIF and NvM.

During the build process, I encountered an error. It appears that the BSW components, particularly MemIF, are expecting a function called "Fee_SetMode" from the Fee module to set mode of Fee is Slow or Fast, which is not provided by the NXP MCAL package.

I'm seeking guidance on how to resolve this error. Is there an alternative solution to address this issue, such as a different function or configuration setting?

Any help or insights would be greatly appreciated!

Thank you.

0 件の賞賛
返信
1 返信

1,642件の閲覧回数
CongDang
NXP Employee
NXP Employee

I guess you are using NXP MCAL package with AUTOSAR CP R21-11 that Fee_Setmode Api is obsolate. So I think you should ask for a suitable Basic Software (BSW) from Vector which is compatible with AUTOSAR CP R21-11.

0 件の賞賛
返信