Error during the run / debugging the code to EVB S32k146

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error during the run / debugging the code to EVB S32k146

1,478 次查看
PU1
Contributor II

Hi ,I just started working on NXP .

During the working on EVB S32K146, i am debugging using the USB.

but not able to debug.

the IDE shows the below pop up  window and the debugging operation stops immediately.

when i try run / debug the code this window pop-upwhen i try run / debug the code this window pop-up

0 项奖励
回复
3 回复数

1,424 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Did you test the S32K1 SDK examples in S32 Design Studio for ARM Version 2.2?

Click Generate Processor Expert Code and then build the project, click debug here:

Debug Configurations.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,351 次查看
PU1
Contributor II
Thanks for reply .
I have tried that also it shows the "DEVICE IS UNSECURED"
and the stops. ask for processing unsecured.
0 项奖励
回复

1,305 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Try to use P&E Recovery Utility halt MCU, and then you should be able to program it. Refer to: S32K144 D2 RED LED is ON always

 

0 项奖励
回复