EMIOS PWM ISSUE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EMIOS PWM ISSUE

1,045 Views
Ayaz
Contributor IV

Hi

I am using EMIOS for  of  PWM  generation ,  I am using this formular:

PWM frequency = CORE_CLK / global prescaler / internal prescaler / (B1+1).

and my configuration is that i am using an external counter buses  A  and F.

The issue i am facing  that when i am trying to use the internal counter or local counter buses the output is not the same as when i am using  an external counter buses A  and F, does it have a different formular?

 

Tags (1)
0 Kudos
Reply
1 Reply

1,020 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please attach two test projects or screenshots of the S32 Configuration Tool configuration so that I can quickly test to see if I can reproduce the phenomenon you mentioned.

Please also tell us the version of S32K3 RTD that you are using. By the way, please also refer to S32K344: Unable to generate complementary PWM signals with 200 Hz in OPWMB mode

Best Regards,
Robin

0 Kudos
Reply