ECDSA verification for imported ECC public key within a X509 certification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ECDSA verification for imported ECC public key within a X509 certification

647 Views
anakha
Contributor III

Hello there,

I am having issue with verification of a certification. Its signature algorithm is SHA256 with ECDSA and use curve as secp256r1.

I am receiving certificate via CAN and store. I wrote a parser to split TBS, public key, signature algorithm and signature itself as R and S values. 

I checked public key, R and S values and their lengths are correct. But EcdsaVerify() function returns HSE_SRV_RSP_VERIFY_FAILED.

What am I doing wrong or am I skip something? 

 

 

 

/* Verify X.509 certificate */

hseSrvResponse_t HseResponse;    
X509_Certificate parsedCert;
if (!X509_ParseCertificate(certificate, length, &parsedCert))
{
   return false; // failed
}
    // extract/parse R and S values
if (!ExtractSignatureRS(parsedCert.signature, parsedCert.signatureLen, &signR_Client, &signRLen_Client, &signS_Client, &signSLen_Client))
{
  return false;
}
    // Check Certificate signature
    /*Loads ECC Public Key stored into the RAM catalog*/
publicKeyEccExt = parsedCert.publicKey;
HseResponse = LoadEccUncompressedExternalPublicKey(&ECCImportedPubHandle, 0, HSE_EC_SEC_SECP256R1, (parsedCert.publicKeyLen / 2 * 8), publicKeyEccExt); //skip 1st byte (0x04) because it represent uncompressed
ASSERT(HSE_SRV_RSP_OK != HseResponse);

HseResponse = ImportFormattedCertEccKeyReq(ECCImportedPubHandle, HSE_KEY_TYPE_ECC_PUB_EXT, HSE_KF_USAGE_VERIFY, HSE_EC_SEC_SECP256R1, (parsedCert.publicKeyLen / 2 * 8), HSE_KEY_FORMAT_ECC_PUB_UNCOMPRESSED, parsedCert.publicKey, parsedCert.tbsCertificateLen, parsedCert.tbsCertificate);
ASSERT(HSE_SRV_RSP_OK != HseResponse);

	/* Verifies the signature with the public Key stored inn the RAM catalog using the signature generated above*/
HseResponse = EcdsaVerify(ECCImportedPubHandle, HSE_HASH_ALGO_SHA2_256, (uint32)parsedCert.tbsCertificateLen, (const uint8*)parsedCert.tbsCertificate, FALSE, 0U, &signRLen_Client, signR_Client, &signSLen_Client, signS_Client);
ASSERT(HSE_SRV_RSP_OK != HseResponse);

 

 

 

 

here are more details for key catalog definition:

 

 

 

#define CRYPTO_START_SEC_CONST_UNSPECIFIED
#include "Crypto_MemMap.h"

/* Table containing RAM key catalog entries */
const hseKeyGroupCfgEntry_t RAM_KeyCatalog[] =
{
    /* RamKeyGroup_RamKey */
    {(HSE_MU0_MASK), HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_AES, 1U, 256U, {0U, 0U}},	/* AES GCM Authentication */
	{HSE_MU0_MASK, HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_ECC_PUB, 1U, HSE_KEY521_BITS, {0U, 0U}}, /* ECC Public Key for signature Group*/
	{HSE_MU0_MASK, HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_ECC_PUB_EXT, 1U, HSE_KEY521_BITS, {0U, 0U}}, /* ECC Public Key for imported certificate Group*/
    /* Marker to end the key catalog */
    {0U, 0U, 0U, 0U, 0U, {0U, 0U}}
};

#define CRYPTO_STOP_SEC_CONST_UNSPECIFIED
#include "Crypto_MemMap.h"

 

 

 

and its handle creation:

 

 

 

ECCImportedPubHandle = GET_KEY_HANDLE(HSE_KEY_CATALOG_ID_RAM,2,0);	//imported ECC public key from certificate

 

 

 

 

other HSE functions like self generate, sign and verification is success using ECC.

I am using RTD 4.0.0. without Autosar with S32K344

 

thanks in advance.

regards,

Tags (4)
0 Kudos
Reply
0 Replies