ECC SRAM Reporting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ECC SRAM Reporting

Jump to solution
2,756 Views
smt87
Contributor II

Hi,

I am using S32K11x MCU for my project. I want to use ECC reporting for safety mechanism, so I want to learn how can i use this safety mechanism and is there any demo code or any application? I would be glad if someone explain to me.

0 Kudos
Reply
1 Solution
2,742 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@smt87

yes ,you can refer to AN12522

Senlent_0-1656999250588.png

 

View solution in original post

Tags (1)
0 Kudos
Reply
5 Replies
2,749 Views
smt87
Contributor II

Hi,

In S32K11x on-chip RAM can be used in following applications:
• Safety critical applications: SRAM_U can be used, which starts from 2000_0000.

So S32k11xx only has SRAM_U for app, right?

0 Kudos
Reply
2,752 Views
Senlent
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
2,605 Views
smt87
Contributor II

Hi,

Do you have any idea how i can check this sample function working correctly?

0 Kudos
Reply
2,747 Views
smt87
Contributor II

Hi,

In S32K11x on-chip RAM can be used in following applications:
Safety critical applications: SRAM_U can be used, which starts from 2000_0000.

So S32k11xx only has SRAM_U for app, right?

0 Kudos
Reply
2,743 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@smt87

yes ,you can refer to AN12522

Senlent_0-1656999250588.png

 

Tags (1)
0 Kudos
Reply