EAR examples problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EAR examples problem

2,553件の閲覧回数
pietroserao
Contributor II

Good evening to everybody.

My name is Pietro, i'm using  S32 Design Studio for ARM Version: 1.2

I'm using an X-FRDMPK144-Q100 NXP Demoboard.

 

I'm trying to run some EAR driver examples but i can't recognize some header libraries.

The missing files are Cpu.h, pin_mux.h, clockMan1.h and flexTimer1.h 

 

 

I show you what i see

168397_168397.jpgmissing libraries.jpg

 

 

How can i find that files? There is a particular setup?

Are that examples suitable for my demoboard?

 

Thank you.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,345件の閲覧回数
raresvasile
NXP Employee
NXP Employee

Hi Pietro,

It seems that the ProcessorExpert configuration files are not generated. 

You can go in the menu bar and select Generate ProcessorExpert Code under project(Please see the attached picture below). This should generate the necessary configuration structures in order to compile the application.

pastedImage_2.png

Please let me know if this was the solution.

Thanks,

Rares

0 件の賞賛
返信

2,345件の閲覧回数
pietroserao
Contributor II

Thank you so much!

It works now :-)

0 件の賞賛
返信