Does the S32K344 example have a simple register version instead of AUTOSAR?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the S32K344 example have a simple register version instead of AUTOSAR?

30,697 Views
xiaoquan
Contributor I

I have the following questions: 1. Does the S32K344 example have a simple register version instead of AUTOSAR (because I only know register manipulation)? Simple register examples like the S32K144 2. Is there a KEIL sample project for S32K344 (preferably including FreeRTOS), if not, can provide a KEIL porting tutorial? THANKS AND PLEASE~

0 Kudos
Reply
8 Replies

30,651 Views
zhang_qazma
Contributor I

S32DS上怎么跑freeRTOS啊,新手一脸懵

0 Kudos
Reply

30,665 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport


If you mean RTD, it integrates both AUTOSAR (formerly MCAL) and non-autosar (formerly) SDK drivers:
https://www.nxp.com/docs/en/product-brief/RTD-S32K3-PB.pdf


Regarding KEIL, their web declares support for this device:
https://www.keil.com/dd2/nxp/s32k344/

0 Kudos
Reply

30,661 Views
xiaoquan
Contributor I

THANKS, 靓仔

0 Kudos
Reply

30,669 Views
xiaoquan
Contributor I

别让它沉下去了,搞起来啊

0 Kudos
Reply

30,671 Views
xiaoquan
Contributor I

官方的靓仔呢?出来说两句?

0 Kudos
Reply

30,671 Views
xiaoquan
Contributor I

DEMO板买不到,芯片买不到,资料好杂乱啊,这款芯片绝了

0 Kudos
Reply

30,671 Views
xiaoquan
Contributor I

有没有KEIL(MDK)+freertos的demo啊? S32K344

0 Kudos
Reply

30,671 Views
xiaoquan
Contributor I

那个靓仔可以告诉我啊

0 Kudos
Reply