S32 Design Studio for S32 Platform v3.4 (Windows/Linux) released!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for S32 Platform v3.4 (Windows/Linux) released!

1,433件の閲覧回数
tom_20xx
Contributor I

I uninstalled the S32 DS 3.4 several days ago, when i reinstall this sw, i can not register it.

I have tried to get a new code by registering a new nxp id with a new email address, but it not work also. 

I think if it is the reason when i uninstalling the S32DS, i did not reinstall very well(e.g return the code)?

My code is C553-F7D3-4E36-7B50, thanks for helping!

0 件の賞賛
返信
2 返答(返信)

1,408件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi Cao,

I reviewed the logs on our activation server, it seems it's not properly generating the activation request. Perhaps this can be solved by re-initializing the trusted storage as follows:

Windows host:

-> Delete 'C:\ProgramData\FLEXNet'

 

This folder may be hidden by default, so then it would be necessary to change Windows Explorer settings to show hidden items.

Linux host:

/usr/local/share/macrovision/storage

 

Best Regards,

Mike

0 件の賞賛
返信

1,417件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Cao,

What error message are you receiving after entering the activation code during installation?

Mike

0 件の賞賛
返信