Does S32K324 support external RAM?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does S32K324 support external RAM?

ソリューションへジャンプ
3,013件の閲覧回数
dmitry_buchynski
Contributor II

Hello.
We use s32k324 in our project but not sure if we have enough RAM for future. Is it possible to use external RAM with this controller? If so, what interface can be used for this purpose and is there an example covering this case?
Best regards.

タグ(3)
0 件の賞賛
返信
1 解決策
2,934件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

We only have the QSPI module, which support the memory mapping (only Reads) with the AHB bus, here the limit is that the external memory has to support the QSPI interface.

Best regards,
Peter

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,977件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

It support external flash or RAM memory with the QSPI interface, but we only have one interface, so not both cases. If you going to use the AHB bus, then the max memory mapped is 128MB.

If the example is not included in S32DS RTD examples then we have not. But I now see it in S32DS RTD for S32K3xx.

Best regards,

Peter

0 件の賞賛
返信
2,965件の閲覧回数
dmitry_buchynski
Contributor II

@petervlna thanks for your reply. I have found the example.
But if I understand the reference manual and example correctly the QSPI only supports memory mapped read operations and does not support memory mapped write. Am I correct? 

0 件の賞賛
返信
2,935件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

We only have the QSPI module, which support the memory mapping (only Reads) with the AHB bus, here the limit is that the external memory has to support the QSPI interface.

Best regards,
Peter

0 件の賞賛
返信