Does S32K provide temperature data?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does S32K provide temperature data?

2,909 Views
stephandewit1
Contributor II

Does the S32K1xx, specifically the S32K148UAT0VLQR, provide any type of temperature data? Perhaps from an internal analog channel or maybe another source?

I thought I remember seeing something of this sort some time ago but I cannot find anything in the reference manual.

Thanks,

Stephan

0 Kudos
Reply
7 Replies

1,984 Views
slevitov
Contributor I

Hi Victor, could you also share the information on internal temp. measurement with me? Thanks in advance. 

0 Kudos
Reply

937 Views
mstroven
Contributor III

I'm just looking for any reference doc that specifies the degrees C / lsb conversion factor for the internal temp reading on S32K1xx

0 Kudos
Reply

924 Views
Matthias_LEHMANN
Contributor III
Hi mstroven,
we've previously used the conversion of NXP's application note AN3031, under the assumption that the S32 would follow a similar behaviour. We've only ever used this function for some quick and dirty engineering assessments and have fairly quickly switched to an external temperature sensor. The readings of the internal sensor also showed some glitches, but that might just be due to the fact, that we didn't put much effort into a robust implementation...
Hope this helps
\\// Matthias

921 Views
mstroven
Contributor III
Thank you much!
0 Kudos
Reply

2,817 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Stephan,

I just sent you an email to discuss this thread privately. For further information, please reply to the email that you received.

Best regards,

Victor

0 Kudos
Reply

2,080 Views
Matthias_LEHMANN
Contributor III
Hi Victor,
although it's already a bit older, I'm hijacking this thread instead of opening a new topic. So far we've already been using the internal temperature sensor of the S32K142 for development purposes. Going forward, we'd also like to use it in a released product. Can you please also provide me this information that's apparently not supposed to be publicly distributed?

Thank you, Matthias
\\// Matthias
0 Kudos
Reply

2,798 Views
paulsiegel
Contributor I

Hello Victor, 

for which reason is this information secret?

I am desperately searching on how to read internal ADC like Bandgap and Temperature.

thank you

Paul

0 Kudos
Reply