Does NXP official have a code routine for configuring external boot for S32K344 chip?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does NXP official have a code routine for configuring external boot for S32K344 chip?

1,061件の閲覧回数
SCoder41
Contributor III

Does NXP official have a code routine and tutorial for configuring external boot for S32K344 chip? We would like to configure the chip to boot from the SD card?

0 件の賞賛
返信
2 返答(返信)

1,024件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

This device does not offer an option to boot from external memory.

Device supports secure and nonsecure boot modes but in both cases it is internal flash boot.

0 件の賞賛
返信

15件の閲覧回数
addisonaudette1
Contributor II

In a nonsecure boot configuration - does the first bootloader run from ROM (is it immutable)?

Can this first bootloader be configured to boot the subsequent bootloaders/application images from an external source/flash?

0 件の賞賛
返信