Does NXP official have a code routine for configuring external boot for S32K344 chip?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does NXP official have a code routine for configuring external boot for S32K344 chip?

1,208 Views
SCoder41
Contributor III

Does NXP official have a code routine and tutorial for configuring external boot for S32K344 chip? We would like to configure the chip to boot from the SD card?

0 Kudos
Reply
2 Replies

1,171 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

This device does not offer an option to boot from external memory.

Device supports secure and nonsecure boot modes but in both cases it is internal flash boot.

0 Kudos
Reply

162 Views
CTCoder1
Contributor II

In a nonsecure boot configuration - does the first bootloader run from ROM (is it immutable)?

Can this first bootloader be configured to boot the subsequent bootloaders/application images from an external source/flash?

0 Kudos
Reply