Disconnecting the external OSC.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Disconnecting the external OSC.

1,297 Views
aboeini
Contributor I

Hello community members,

I am working on S32K, I wanted to disconnect the external oscillator on the HW. I want to just use FIRC as the main clock. But we have issues with this. 

I just want to understand, is this possible? 

I configured SCG_RCCR to use FIRC. which means the system clock is provided by FIRC. When I had to configure the CAN clock source I selected 1 to use SYS_CLK.

Please provide your inputs.

Thank you

Tags (2)
0 Kudos
Reply
1 Reply

1,286 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @aboeini,

The SOSC clock is recommended because of the FIRC tolerance.

danielmartynek_0-1622554183031.png

Please refer to: CAN with Flexible Data-Rate Specification Version 1.0 

p. 32 Oscillator Tolerance

FlexCAN Bit Timing Calculation 

STEP 6: Calculate required oscillator tolerance

You can use this calculator to calculate the df(%).

MPC5xxx/S32Kxx: CAN / CAN FD bit timing calculation 

 

Regards,

Daniel

 

 

0 Kudos
Reply