Disabling Global Interrupts inside ISR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Disabling Global Interrupts inside ISR

ソリューションへジャンプ
3,440件の閲覧回数
Maciek
Contributor V

Hi,

we have an application (S32K118 - Cortex-M0+) where a few parameters can be changed upon the request via CAN or UART. The requests set the global variables inside the Receive ISR.
Subsequently, the highest priority (lowest importance) PIT Timer ISR reads those variables. To ensure the data integrity we want to temporarily switch off ALL the Interrupts while reading the global variables inside Timer ISR. Is it safe/recommended to use DISABLE_INTERRUPTS() just before reading globals inside Timer ISR and to call ENABLE_INTERRUPTS() just after the reading - to make a kind of 'critical section' this way ?

What about memory and instruction barriers like  __DSB() and __ISB() - should we use them (it's Cortex-M0+) in this case ?
Will it change if we would like to switch off only particular Interrupts (like CAN receive interrupt) ?

 Are there any differences if we want to apply above solution in case of i.MX RT (Cortex-M7) ?

Thanks

Maciek

0 件の賞賛
返信
1 解決策
3,421件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Maciek,

I don't see any issue with that.

The interrupt can be preempted only by an interrupt with a higher priority.

So, you can mask the interrupt globally as you mentioned.

 

Regarding the barriers, please refer to this document:

ARM Cortex ™ -M Programming Guide to Memory Barrier Instructions Application Note 321

https://documentation-service.arm.com/static/5efefb97dbdee951c1cd5aaf?token=

4.8 Disabling interrupts using CPS and MSR instructions
4.7 Enabling interrupts using CPS instructions and MSR instructions

 

There are no errata related to this:

https://www.nxp.com/docs/en/errata/S32K118_0N97V.pdf

 

I'm not familiar with i.MX RT, please create a new thread on the i.MX RT community.

 

Regards,

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,422件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Maciek,

I don't see any issue with that.

The interrupt can be preempted only by an interrupt with a higher priority.

So, you can mask the interrupt globally as you mentioned.

 

Regarding the barriers, please refer to this document:

ARM Cortex ™ -M Programming Guide to Memory Barrier Instructions Application Note 321

https://documentation-service.arm.com/static/5efefb97dbdee951c1cd5aaf?token=

4.8 Disabling interrupts using CPS and MSR instructions
4.7 Enabling interrupts using CPS instructions and MSR instructions

 

There are no errata related to this:

https://www.nxp.com/docs/en/errata/S32K118_0N97V.pdf

 

I'm not familiar with i.MX RT, please create a new thread on the i.MX RT community.

 

Regards,

Daniel

0 件の賞賛
返信