Disable Multi-Bit ECC Error Exception

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Disable Multi-Bit ECC Error Exception

1,009 Views
paul_jack
Contributor I

Hello everyone, when I used UDSboot to test the update program, a Multi-Bit ECC Error occurred, which caused the program to get stuck in the hardware fault handler and could not update the program again through UDSboot. Then I configured PFCR[DMEEE] to 1, which could solve the problem of getting stuck. I wonder if the official advice is to Disable Multi-Bit ECC Error Exception?

0 Kudos
Reply
0 Replies