Demo Code for s32k148

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Demo Code for s32k148

4,366件の閲覧回数
bradford96789
Contributor I

Has the demo code for the s32k148 board been released yet? If so, where can I find it? And if not, when will it be released?

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

4,033件の閲覧回数
nelson_lin
Contributor I

dianabatrlova‌

The link below is for AN5408SW.

AN5413SW:

https://www.nxp.com/webapp/Download?colCode=AN5408SW

When I try https://www.nxp.com/webapp/Download?colCode=AN5413SW, this site can’t be reached.

May you help me out?

Best Regards,

Nelson

0 件の賞賛
返信

4,033件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Nelson,

You are right. Unfortunately, the software for the AN5413 was removed and this software is not possible to download from the NXP site. (I assume because of some updates). In the meantime use the link below.

https://source.codeaurora.org/external/s32support/S32K1xx_cookbook/

I hope it helps.

Best Regards,

Diana

0 件の賞賛
返信

4,033件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Bradford,

The demo applications can be found in the AN5413:

https://www.nxp.com/docs/en/application-note/AN5413.pdf 

AN5413SW:

https://www.nxp.com/webapp/Download?colCode=AN5408SW 

Other documents related to S32K, see in section Application Notes on the link below:

32-bit Automotive General Purpose MCUs|NXP 

Also, you can look at the demo codes in the S32 Design studio for ARM 2018.R1 in File -> New -> 32DS Project from Example.

https://www.nxp.com/docs/en/application-note/AN5413.pdf

I believe it helps you.

Best Regards,

Diana

0 件の賞賛
返信