Delay of LPSPI between frames

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Delay of LPSPI between frames

1,760 Views
fumiaki
Contributor I

Regarding to the delay such PCSSCK, SCKPCS and DBT of S32K144 LPSPI CCR, SCKPCS in reference manual states "configures the delay from the last SCK edge to the PCS negation".

 

Even without PCS negation between frames, do the delays occur correctly?

When CS has been kept assertion between frames using GPIO, it seemed ​like the delays occurred.

0 Kudos
Reply
1 Reply

1,749 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @fumiaki,

The LPSPI module does not have an option to disable the PCS.

So even if you don't use the PCS output of the LPSPI module on a port but you use a GPIO instead, the module still keeps generating it with the configurable delay.   

 

Regards,

Daniel

0 Kudos
Reply