Delay of LPSPI between frames

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Delay of LPSPI between frames

1,759件の閲覧回数
fumiaki
Contributor I

Regarding to the delay such PCSSCK, SCKPCS and DBT of S32K144 LPSPI CCR, SCKPCS in reference manual states "configures the delay from the last SCK edge to the PCS negation".

 

Even without PCS negation between frames, do the delays occur correctly?

When CS has been kept assertion between frames using GPIO, it seemed ​like the delays occurred.

0 件の賞賛
返信
1 返信

1,748件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @fumiaki,

The LPSPI module does not have an option to disable the PCS.

So even if you don't use the PCS output of the LPSPI module on a port but you use a GPIO instead, the module still keeps generating it with the configurable delay.   

 

Regards,

Daniel

0 件の賞賛
返信