DebuggerHeldCoreLoop

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DebuggerHeldCoreLoop

2,616件の閲覧回数
zhiguoguo
Contributor I

zhiguoguo_0-1661428796265.pngzhiguoguo_0-1661428796265.png

Hello.

When I was learning S32DS Startup_cm7.s files, I encountered a problem. I can't understand the function shown in the picture above.

First :What is the function of DebuggerHeldCoreLoop?

Second: RESET_CATCH_CORE is an Random number or Specific number?

Three: Why compare R0 with 0x5A5A5A5A?

 

Expect to receive a reply.

thanks

 

 

0 件の賞賛
返信
3 返答(返信)

2,597件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @zhiguoguo,

As you can see in the system.c file

danielmartynek_0-1661759096695.pngdanielmartynek_0-1661759096695.png

The RESET_CATCH_CORE variable can be overwritten by the debugger to 0x5A5A5A5A, which will catch the execution in that loop.

 

Regards,

Daniel

0 件の賞賛
返信

2,584件の閲覧回数
zhiguoguo
Contributor I

if I want to migrate project to IAR,what modify I need to this value?

タグ(1)
0 件の賞賛
返信

2,571件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @zhiguoguo,

I would recommend contacting IAR Systems.

 

Thanks,

Daniel

0 件の賞賛
返信