Debugger Cable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugger Cable

1,134 Views
Prajwal123
Contributor II

I want to connect the segger 20-pin J-Link pro debugger to S32K148EVB JTAG header. The pitch size of the S32K148EVB JTAG header is 1.27mm(0.05") whereas the size of the J-Link pro is 2.54mm(0.1"). Can I use the " J-Link 19-pin Cortex-M Adapter: Adapts from 20
pin, 0.1' Standard connector to 19-pin, 0.05' Cortex
M connector incl. 19 pin cable" to connect the J-Link pro debugger to the JTAG header in S32K148EVB?

0 Kudos
Reply
2 Replies

1,105 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

https://www.segger.com/products/debug-probes/j-link/accessories/adapters/19-pin-cortex-m-adapter/

This can be used to debug S32K148.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,133 Views
Prajwal123
Contributor II

For debugging

Tags (1)
0 Kudos
Reply