Debug problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug problem

11,005 Views
Hermit
Contributor I

Dear Team,

I want to debug the project on S32K342. However, some errors appeared. I attached the screenshot.  And the debugger I used is PE micro multilink.

0 Kudos
Reply
5 Replies

10,973 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Hermit 

To confirm, when developing an Arm® circuit board, it is recommended to use a standard debug signal arrangement to make a connection to the debugger easier, as it is shown in the below image:

VaneB_0-1675113424123.pngVaneB_0-1675113424123.png

The connections were made in this way. If not, could you share how you have the debugger connection?

 

B.R.

VaneB

 

0 Kudos
Reply

10,957 Views
Hermit
Contributor I

Hi VaneB,

The error I metioned before has been resolved by adjusting the speed. However, there are some new errors appearing. I attached the screenshots below. Hope your response.

 

Best Regards,

Hermit

0 Kudos
Reply

10,944 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Hermit 

Could you share with me your hardware connections?

0 Kudos
Reply

10,928 Views
Hermit
Contributor I

Hi VaneB

The problem has been resolved. Thanks.

 

Best regards,

Hermit

0 Kudos
Reply

10,961 Views
Hermit
Contributor I

Hi VaneB,

I have ensured that our connections are similarly to what you offered. Is there any other configuration I should perform to make it successful? For example,the speed?

 

Regards,

Hermit

0 Kudos
Reply