Debug issue - EVB S32K116-Q048

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug issue - EVB S32K116-Q048

1,884件の閲覧回数
pawl
Contributor I

Hello,

I am trying to run eval board XS32K116EVB2Q048. I am not able to flash/debug it with S32 Design Studio for ARM Version 2.2. I based on Getting Started instruction.

Jumper settings:

J104 2-3

J107 2-3 (S32K11x powered by USB micro connector)

J10 2-3

J108, J15 1-2

 

Project setting:

pawl_1-1704731744537.png

 

pawl_2-1704731751442.png

Progress got stuck on 62%:

pawl_3-1704731765640.png


FreeMaster connection error:

pawl_4-1704731783333.png

Board appears as mass storage device in PC, but I haven’t seen toggle RGB (preloaded software).

Best regards,
Pawel

0 件の賞賛
返信
3 返答(返信)

1,818件の閲覧回数
pawl
Contributor I

It was related to Windows administrator rights. Debugger is working good now.

0 件の賞賛
返信

1,863件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@pawl

I followed your steps to try to reproduce your problem, but everything works fine on myside.

1.Can you try a few more times? This may be due to your PC.

2.Please make sure S32K116 has been programmed correctly "S32K116_EVB_JumpStart_Firmware"

S32K116_EVB_JumpStart_Firmware
What I need to tell you is that this routine is based on a very early version of hardware and software. It does not work perfectly with the new version of S32K116EVB, but I have tested it and at least the connection can work.

0 件の賞賛
返信

1,614件の閲覧回数
reidefe
Contributor I

Please i am having the same issue with the same board. Not recognized on Freemaster, and s32ds for arm recognizes it as a different SKU but debugging is still impossible. Implemented the "S32K116_EVB_JumpStart_Firmware" update by copying the .srec file into the device USB folder. 
Currently, all it does is make the LED light blink 8 times then a 2-second pause on repeat. 

0 件の賞賛
返信