DMA+ADC IN VLPS mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DMA+ADC IN VLPS mode

1,257 Views
YASHAY
Contributor I

Hi,

can i use DMA+ADC  on S32K116 micro in VLPS mode ?

reading some documents it seems you can use but it does not give me the option on S32K Power estimation tool ?

need some guidance.

Thanks.

0 Kudos
Reply
3 Replies

1,227 Views
YASHAY
Contributor I

Thanks for the reply.

so in order to use ADC+DMA for minimum power consumption , i have to change power mode every time?

in RUN mode using only ADC and DMA what could be the typical current consumption do you have any idea ? 

Thanks

 

0 Kudos
Reply

1,205 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Yes, ADC is not available in VLPS, so you need to change the mode. I don't know current consumption for this exact use-case, I can only recommend "Table 13. Power consumption" in the datasheet and Power Estimation Tool to get some boundaries what to expect.

Regards,

Lukas

0 Kudos
Reply

1,237 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @YASHAY 

you can take a look at "Table 39-4. Module operation in available power modes" in the reference manual:

https://www.nxp.com/webapp/Download?colCode=S32K1XXRM

It says that ADC is turned off in VLPS mode:

lukaszadrapa_0-1698123101439.png

 Regards,

Lukas

0 Kudos
Reply