Crypto Stack - Key Exchange Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Crypto Stack - Key Exchange Configuration

ソリューションへジャンプ
4,243件の閲覧回数
Yetkin
Contributor I

Hi,

I need to implement ECDH (Eliptic Curve Diffie Hellman) to perform key exchange. However, there is no CRYPTO_ALGOFAM_ECDH parameter for CryptoPrimitiveAlgorithmFamily in Crypto Driver configurations, because I am using AUTOSAR 4.3. Is there a way to implement ECDH in accordance with AUTOSAR 4.3 or I have to use Ed25519 ?   

0 件の賞賛
返信
1 解決策
4,075件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hi @Yetkin,

There are no S32K3 packages for AUTOSAR 4.3

With ECDH for AUTOSAR 4.4, I attached an example built on the SAF85_S32R41_RTD_0_9_0_D2207 package. You can port this example for the S32K3 RTD package.

Password: NXP

Best regards,

Dan

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,205件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hello @Yetkin,

what is the package you are using?

Best regards,

Dan

0 件の賞賛
返信
4,195件の閲覧回数
Yetkin
Contributor I

Hi,

I am using the MCAL package SW32K3_RTD_4.4_R21-11_3.0.0_P01_HF02.

0 件の賞賛
返信
4,076件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hi @Yetkin,

There are no S32K3 packages for AUTOSAR 4.3

With ECDH for AUTOSAR 4.4, I attached an example built on the SAF85_S32R41_RTD_0_9_0_D2207 package. You can port this example for the S32K3 RTD package.

Password: NXP

Best regards,

Dan

0 件の賞賛
返信
4,059件の閲覧回数
Yetkin
Contributor I

Hi,

Thank you, it helped me much.

Best regards,

Yetkin

0 件の賞賛
返信