Continuous adc conversion for multiple channels using SW Trigger in S32k

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Continuous adc conversion for multiple channels using SW Trigger in S32k

1,282 Views
Guna
Contributor I

Hello everyone,

I am currently checking adc using SW trigger. As per my requirement, the SW trigger was working properly by calling AdcStartGroupConversion(). which will be called multiple times in a function. Currently, I have added some more channels to the same group. but this time it is not working; it is converting only once after that it is not, even though if I call AdcStartGroupConversion() multiple times. Also, I have other 2 groups with the same configuration and with SW triggers that are converting multiple times. I'm confused now as to why it is not working as expected. 

I verified all my configurations with other working groups, which are the same. The major change that I have made is adding two more channels to that group. Any idea what is the reason behind this?

 

0 Kudos
Reply
1 Reply

1,248 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Guna

Could you please tell me the part number you're using? and the SDK and IDE version.

Aslo please provided me your project and i will help you to check it.

0 Kudos
Reply