Connection problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connection problem

2,778件の閲覧回数
d_shivamkumar
Contributor III

recently i was trying to do some memory functions with my S32K144EVB. by mistake, I have erased the entire p-flash memory. since then I am unable to load any programs to the board. every time I'm trying to do so the error shows that I am not able to connect with the board. additionally, the red LED near to MicroUSB (usual programming interface) is continuously on. please help me to resolve this. is this end of life for this EVB?

0 件の賞賛
返信
3 返答(返信)

2,741件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

It is hard to say, it could be anything.

Even the OpenSDA debugger can be damaged.

Can you measure the J15 VDD_MCU power supply?

Is the board heating?

 

Thank you,

Daniel

0 件の賞賛
返信

2,760件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

Can you show the error message that you get from the debugger?

Do you have any other debugger?

Before you erased the PFlash, was the MCU partitioned for CSEc?

 

Thank you,

BR, Daniel

0 件の賞賛
返信

2,756件の閲覧回数
d_shivamkumar
Contributor III

d_shivamkumar_0-1602155370058.pngd_shivamkumar_0-1602155370058.png

it is not going beyond this point even after frequent retry.

i don't have any other debugger.

MCU wasn't partitioned for CSEc.

 

0 件の賞賛
返信