Connection problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connection problem

3,003 Views
d_shivamkumar
Contributor III

recently i was trying to do some memory functions with my S32K144EVB. by mistake, I have erased the entire p-flash memory. since then I am unable to load any programs to the board. every time I'm trying to do so the error shows that I am not able to connect with the board. additionally, the red LED near to MicroUSB (usual programming interface) is continuously on. please help me to resolve this. is this end of life for this EVB?

0 Kudos
Reply
3 Replies

2,966 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

It is hard to say, it could be anything.

Even the OpenSDA debugger can be damaged.

Can you measure the J15 VDD_MCU power supply?

Is the board heating?

 

Thank you,

Daniel

0 Kudos
Reply

2,985 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

Can you show the error message that you get from the debugger?

Do you have any other debugger?

Before you erased the PFlash, was the MCU partitioned for CSEc?

 

Thank you,

BR, Daniel

0 Kudos
Reply

2,981 Views
d_shivamkumar
Contributor III

d_shivamkumar_0-1602155370058.png

it is not going beyond this point even after frequent retry.

i don't have any other debugger.

MCU wasn't partitioned for CSEc.

 

0 Kudos
Reply