Connection problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Connection problem

1,907 次查看
d_shivamkumar
Contributor III

recently i was trying to do some memory functions with my S32K144EVB. by mistake, I have erased the entire p-flash memory. since then I am unable to load any programs to the board. every time I'm trying to do so the error shows that I am not able to connect with the board. additionally, the red LED near to MicroUSB (usual programming interface) is continuously on. please help me to resolve this. is this end of life for this EVB?

0 项奖励
回复
3 回复数

1,870 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

It is hard to say, it could be anything.

Even the OpenSDA debugger can be damaged.

Can you measure the J15 VDD_MCU power supply?

Is the board heating?

 

Thank you,

Daniel

0 项奖励
回复

1,889 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

Can you show the error message that you get from the debugger?

Do you have any other debugger?

Before you erased the PFlash, was the MCU partitioned for CSEc?

 

Thank you,

BR, Daniel

0 项奖励
回复

1,885 次查看
d_shivamkumar
Contributor III

d_shivamkumar_0-1602155370058.png

it is not going beyond this point even after frequent retry.

i don't have any other debugger.

MCU wasn't partitioned for CSEc.

 

0 项奖励
回复