Connecting to target

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connecting to target

1,276 Views
lohrsistemas
Contributor IV

After some burnnings my MCU stopped responding. Giving the following error:
Connecting to J-Link ...
J-Link is connected.
Firmware: J-Link ARM V7 compiled Jun 20 2012 19:45:53
Hardware: V7.00
S / N: 157001692
OEM: IAR
Checking target voltage ...
Target voltage: 5.12 V
Listening on TCP / IP port 2331
Connecting to target ... ERROR: Kinetis (connect): Timeout while halting CPU. CPU does not stop.

ERROR: Kinetis (connect): Timeout while halting CPU. CPU does not stop.

Any idea what's going on?

0 Kudos
Reply
0 Replies