Connecting to target

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Connecting to target

1,278 次查看
lohrsistemas
Contributor IV

After some burnnings my MCU stopped responding. Giving the following error:
Connecting to J-Link ...
J-Link is connected.
Firmware: J-Link ARM V7 compiled Jun 20 2012 19:45:53
Hardware: V7.00
S / N: 157001692
OEM: IAR
Checking target voltage ...
Target voltage: 5.12 V
Listening on TCP / IP port 2331
Connecting to target ... ERROR: Kinetis (connect): Timeout while halting CPU. CPU does not stop.

ERROR: Kinetis (connect): Timeout while halting CPU. CPU does not stop.

Any idea what's going on?

0 项奖励
回复
0 回复数