Clock Configuration of S32K14x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Clock Configuration of S32K14x

ソリューションへジャンプ
2,366件の閲覧回数
patil_digambar
Contributor I

Hello NXP team,

I am working on S32K14x board, to do MCAL configurations we are using NXP IDE with Processor Expert as well as EB Tresos (for two different projects).

In Processor Expert it is allowing SPLL DIV2 clock frequency as 80Mhz as shown in snap.

Processor Expert ConfigurationProcessor Expert Configuration

But EB Tresos is giving out of range error 

EB Tresos ConfigurationEB Tresos Configuration

 

Can anyone please clarify this; as we want to use this frequency range for our use.

Thank You in Advance.

0 件の賞賛
返信
1 解決策
2,357件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi patil_digambar,

Sorry for the inconvenience we bring you!

The SPLLDIV2_CLK should be configured to 40 MHz or less in RUN mode and 56 MHz or less in HSRUN mode.

SPLLDIV2_CLK.png

EB Tresos is correct.

McuSPLLDiv2Frequency.png

S32 Design Studio for ARM Version 2.2 with Processor Expert was error.
The latest S32 Design Studio for S32 Platform 3.3 with S32_SDK_S32K1xx_RTM_4.0.0 has corrected this error.

S32 Design Studio for S32 Platform 3.3.png

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,351件の閲覧回数
patil_digambar
Contributor I

Thank you Robin

0 件の賞賛
返信
2,358件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi patil_digambar,

Sorry for the inconvenience we bring you!

The SPLLDIV2_CLK should be configured to 40 MHz or less in RUN mode and 56 MHz or less in HSRUN mode.

SPLLDIV2_CLK.png

EB Tresos is correct.

McuSPLLDiv2Frequency.png

S32 Design Studio for ARM Version 2.2 with Processor Expert was error.
The latest S32 Design Studio for S32 Platform 3.3 with S32_SDK_S32K1xx_RTM_4.0.0 has corrected this error.

S32 Design Studio for S32 Platform 3.3.png

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信