Circular buffer using MBDT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Circular buffer using MBDT

1,652件の閲覧回数
rolo90
Contributor I

Hello everyone,

My application needs to write to EEPROM every 1s, and as to not wear the internal EEPROM from the S32K144, I would need to implement a circular buffer. Since there are no "Circular buffer" MBDT blocks, do I need to write custom C code to access specific registers?

Thanks,

Rolando

0 件の賞賛
返信
1 返信

1,639件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Rolando,

For MBDT support, we have currently only the MBDT community.
Can you please post this issue there?
The community is monitored by our MBDT team.
Thank you for your understanding.

Since I am not familiar with MBDT, I don’t know if MBDT can’t achieve this function.
About how to use the EEPROM, please refer: AN11983 Using the S32K1xx EEPROM Functionality

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信