The details about this question is as follows:
MCU: S32K148 in 144 pin backage on a custom designed board.
JTAG: JLink Plus in 10 pin configuration
IDE: S32DS 3.6.2 On Windows 11
Embedded OS: Bare metal with RTD 3.0.0
The board in question is a copy-paste design of a previously working version. However, I cannot write to flash over the JTAG; the readback is all 0xFF.
The JTAG pinout is as shown below:
durga_choudhury_0-1770336172776.png
And on the MCU, they are routed as follows:
TMS (JTAG pin 2) is connected to MCU pin 142 (JTAG_TMS)
TCK (JTAG pin 4) is connected to MCU pin 140 (JTAG_TCLK)
nRESET (JTAG pin 10) is connected to MCU pin 141 (reset_b)
TDO (JTAG pin 6) is connected to MCU pin 136 (JTAG_TDO)
TDI (JTAG pin 6) is connected to MCU pin 139 (JTAG_TDI)
Vref (JTAG pin 1) is connected to 3.3V) (as evidenced by the LED on the JLINK turning green at the start of a code download and staying orange'ish (i.e. both red and green on) at connection, also Jlink confirms that the target voltage is 3.3V)
The pull up/down values are as per the schematic above.
With this, I am not able to write to the flash. After code download, the memory regions just written as read back as 0xFF.
The output from Jlink is as follows:
J-Link>showhwstatus
VTref=3.341V
ITarget=0mA
TCK=1 TDI=0 TDO=1 TMS=0 TRES=1 TRST=1
Supported target interface speeds:
- 180 MHz/n, (n>=12). => 15000kHz, 13846kHz, 12857kHz, ...
- Adaptive clocking
J-Link>connect
Device "S32K148" selected.
Connecting to target via JTAG
ConfigTargetSettings() start
ConfigTargetSettings() end - Took 4us
InitTarget() start
JTAG selected. Identifying JTAG Chain...
TotalIRLen = 4, IRPrint = 0x01
JTAG chain detection found 1 devices:
#0 Id: 0x0995001D, IRLen: 04, JTAG-DP
JTAG Chain Identified. Connecting to DAP TAP...
Successfully connected to selected DAP TAP.
InitTarget() end - Took 55.4ms
TotalIRLen = 4, IRPrint = 0x01
JTAG chain detection found 1 devices:
#0 Id: 0x0995001D, IRLen: 04, JTAG-DP
DPv0 detected
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set, ADDR: 0x00000000)
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FF000
CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)
Found Cortex-M4 r0p1, Little endian.
FPUnit: 6 code (BP) slots and 2 literal slots
CoreSight components:
ROMTbl[0] @ E00FF000
[0][0]: E000E000 CID B105E00D PID 000BB00C SCS-M7
[0][1]: E0001000 CID B105E00D PID 003BB002 DWT
[0][2]: E0002000 CID B105E00D PID 002BB003 FPB
[0][3]: E0000000 CID B105E00D PID 003BB001 ITM
[0][4]: E0040000 CID B105900D PID 000BB9A1 TPIU
[0][5]: E0041000 CID B105900D PID 000BB925 ETM
Memory zones:
Zone: "Default" Description: Default access mode
Cortex-M4 identified.
J-Link>
What could be going wrong?