Can not new a s32k144 project with sdk s32k1 RTD AUTOSAR 4.4 Version 1.0.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not new a s32k144 project with sdk s32k1 RTD AUTOSAR 4.4 Version 1.0.1

Jump to solution
1,395 Views
laofu
Contributor II

Hi@nxp

i have installed s32k1 RTD AUTOSAR 4.4 Version 1.0.1 as follow,

laofu_0-1676547182974.png

 

why i can not import this sdk when new a project.

laofu_1-1676547321184.png

 

Tags (1)
0 Kudos
Reply
1 Solution
1,309 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

please make sure that you choose correct build toolchain. RTD supports GNU gcc v9.2:

jiri_kral_0-1676899478701.png

 

jiri_kral_1-1676899529347.png

 

 

 

View solution in original post

4 Replies
1,310 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

please make sure that you choose correct build toolchain. RTD supports GNU gcc v9.2:

jiri_kral_0-1676899478701.png

 

jiri_kral_1-1676899529347.png

 

 

 

1,230 Views
laofu
Contributor II

I have solved with the help of you ,thanks very much @jiri_kral ,in addition ,do this version  RTD carrying FreeRTOS submodule

0 Kudos
Reply
1,356 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

This could be cause by version of S32 design studio.

Which version of S32DS are you using?

Best regards,

Peter

0 Kudos
Reply
1,349 Views
laofu
Contributor II

it is s32ds 3.4,but i can import example project that use this RTD

thinks 

0 Kudos
Reply