Can not creat a project with S32K342

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not creat a project with S32K342

3,729 Views
Hermit
Contributor I

Hi Team,

I want to creat a new project with S32K342, but I failed. There is no S32K342 chip for me to choose(I attached a screenshot below). 

The version of S32DS is V3.4 and the version of RTD SDK is "SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204". By the way, I can not open the example where S32K342 is used. There is no example for S32K342! I attached it below.

Need I configure the S32DS or add some special packages to make it applicable to S32K342?

0 Kudos
Reply
4 Replies

3,716 Views
Hermit
Contributor I

Thank you

0 Kudos
Reply

3,721 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

be sure right development package is installed into S32DS.

PetrS_0-1673948805896.png

I can see S32K342 option when creating new project

PetrS_1-1673948843804.png

There are examples for S32K342 within RTD package

PetrS_2-1673949469782.png

BR, Petr

 

0 Kudos
Reply

2,777 Views
fan1234
Contributor II

Hi, PetrS

 I can see S32K342 option when creating new project but there are examples for S32K342 within RTD package. can you help me with that?

The version of S32DS is V3.5  and the extension are:

fan1234_0-1733983230675.png

and i checked, thedevelopment package is installed

fan1234_2-1733983461366.png

 

thank you.

Tags (1)
0 Kudos
Reply

2,772 Views
fan1234
Contributor II
sorry, made a mistake,it should be " there are no examples for S32K342 within RTD package".
0 Kudos
Reply