Can not creat a project with S32K342

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can not creat a project with S32K342

3,887 次查看
Hermit
Contributor I

Hi Team,

I want to creat a new project with S32K342, but I failed. There is no S32K342 chip for me to choose(I attached a screenshot below). 

The version of S32DS is V3.4 and the version of RTD SDK is "SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204". By the way, I can not open the example where S32K342 is used. There is no example for S32K342! I attached it below.

Need I configure the S32DS or add some special packages to make it applicable to S32K342?

0 项奖励
回复
4 回复数

3,874 次查看
Hermit
Contributor I

Thank you

0 项奖励
回复

3,879 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

be sure right development package is installed into S32DS.

PetrS_0-1673948805896.png

I can see S32K342 option when creating new project

PetrS_1-1673948843804.png

There are examples for S32K342 within RTD package

PetrS_2-1673949469782.png

BR, Petr

 

0 项奖励
回复

2,935 次查看
fan1234
Contributor III

Hi, PetrS

 I can see S32K342 option when creating new project but there are examples for S32K342 within RTD package. can you help me with that?

The version of S32DS is V3.5  and the extension are:

fan1234_0-1733983230675.png

and i checked, thedevelopment package is installed

fan1234_2-1733983461366.png

 

thank you.

标记 (1)
0 项奖励
回复

2,930 次查看
fan1234
Contributor III
sorry, made a mistake,it should be " there are no examples for S32K342 within RTD package".
0 项奖励
回复