Can S32K116 change the I/O drive current?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can S32K116 change the I/O drive current?

ソリューションへジャンプ
1,269件の閲覧回数
jingfang
Contributor IV

Can S32K116 change the I/O drive current?

 

0 件の賞賛
返信
1 解決策
1,223件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this is Ioh/Iol values for different pad types and DSE setting (where applicable)

PetrS_0-1675245507627.png

BR, Petr

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
1,255件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, this is possible using PORT_PCRn[DSE] bit.
But note, not all pin control settings mentioned in PORT_PCRn register are configurable for all pins. Refer 'Bits Configurable' field in 'IO Signal Table' tab of IO Signal Description Input Multiplexing sheet(s) attached to the Reference Manual. DSE is available for GPIO-HD pad type only.

BR, Petr

0 件の賞賛
返信
1,246件の閲覧回数
jingfang
Contributor IV

How about output current?

Only see high or low.

Some friends of the Mcu chip has value to turn.

c43dcf1d-21b5-4435-af86-198eb6706f6f.jpg 

0 件の賞賛
返信
1,242件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

that is not an option here, current specification is given in the DC electrical specifications sections of the device datasheet.

BR, Petr

0 件の賞賛
返信
1,227件の閲覧回数
jingfang
Contributor IV

Thanks a lot~

What is different between "GPIO-HD_DSE_0" and "GPIO-FAST_DSE_0"?

企业微信截图_16752209043739.png

0 件の賞賛
返信
1,224件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this is Ioh/Iol values for different pad types and DSE setting (where applicable)

PetrS_0-1675245507627.png

BR, Petr

0 件の賞賛
返信