Can S32K116 change the I/O drive current?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can S32K116 change the I/O drive current?

Jump to solution
1,216 Views
jingfang
Contributor IV

Can S32K116 change the I/O drive current?

 

0 Kudos
Reply
1 Solution
1,170 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this is Ioh/Iol values for different pad types and DSE setting (where applicable)

PetrS_0-1675245507627.png

BR, Petr

View solution in original post

0 Kudos
Reply
5 Replies
1,202 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, this is possible using PORT_PCRn[DSE] bit.
But note, not all pin control settings mentioned in PORT_PCRn register are configurable for all pins. Refer 'Bits Configurable' field in 'IO Signal Table' tab of IO Signal Description Input Multiplexing sheet(s) attached to the Reference Manual. DSE is available for GPIO-HD pad type only.

BR, Petr

0 Kudos
Reply
1,193 Views
jingfang
Contributor IV

How about output current?

Only see high or low.

Some friends of the Mcu chip has value to turn.

c43dcf1d-21b5-4435-af86-198eb6706f6f.jpg 

0 Kudos
Reply
1,189 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

that is not an option here, current specification is given in the DC electrical specifications sections of the device datasheet.

BR, Petr

0 Kudos
Reply
1,174 Views
jingfang
Contributor IV

Thanks a lot~

What is different between "GPIO-HD_DSE_0" and "GPIO-FAST_DSE_0"?

企业微信截图_16752209043739.png

0 Kudos
Reply
1,171 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this is Ioh/Iol values for different pad types and DSE setting (where applicable)

PetrS_0-1675245507627.png

BR, Petr

0 Kudos
Reply