Can S32K116 change the I/O drive current?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can S32K116 change the I/O drive current?

跳至解决方案
1,217 次查看
jingfang
Contributor IV

Can S32K116 change the I/O drive current?

 

0 项奖励
回复
1 解答
1,171 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this is Ioh/Iol values for different pad types and DSE setting (where applicable)

PetrS_0-1675245507627.png

BR, Petr

在原帖中查看解决方案

0 项奖励
回复
5 回复数
1,203 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, this is possible using PORT_PCRn[DSE] bit.
But note, not all pin control settings mentioned in PORT_PCRn register are configurable for all pins. Refer 'Bits Configurable' field in 'IO Signal Table' tab of IO Signal Description Input Multiplexing sheet(s) attached to the Reference Manual. DSE is available for GPIO-HD pad type only.

BR, Petr

0 项奖励
回复
1,194 次查看
jingfang
Contributor IV

How about output current?

Only see high or low.

Some friends of the Mcu chip has value to turn.

c43dcf1d-21b5-4435-af86-198eb6706f6f.jpg 

0 项奖励
回复
1,190 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

that is not an option here, current specification is given in the DC electrical specifications sections of the device datasheet.

BR, Petr

0 项奖励
回复
1,175 次查看
jingfang
Contributor IV

Thanks a lot~

What is different between "GPIO-HD_DSE_0" and "GPIO-FAST_DSE_0"?

企业微信截图_16752209043739.png

0 项奖励
回复
1,172 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this is Ioh/Iol values for different pad types and DSE setting (where applicable)

PetrS_0-1675245507627.png

BR, Petr

0 项奖励
回复