Calculation of SOC measurement in Self Discharge mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Calculation of SOC measurement in Self Discharge mode

964 Views
thailivenkatesh8
Contributor II

Dear Sir,
              Using MC33771C BCC driver calculated SOC using coulomb count method. For fully charged battery SOC is 100%.When the controller is in sleep mode(STOP1 power mode)that time we have self discharge & AH decrease in battery pack. But my battery pack showing 100% even if self discharge for long time how to correct this decreased Ah to SOC & estimate the proper SOC.

 

Thanks & Regards,

Venkatesh

0 Kudos
Reply
1 Reply

941 Views

Hello Venkatesh,

If your battery pack is not used for a long time, I would recommend to recalibrate the SOC by performing an open circuit voltage (OCV) measurement before the battery is used again. This will give you a pretty accurate indication of the battery SOC.

The self discharge could also be estimated provided your MCU has a RTC and is able to compute how long the battery has been in idle mode. If you have a modeling of the discharge over time of your battery, you can easily compute the self discharge of the idle time. But I would rely better on the first method because self-discharge is quite temperature dependant and temperature is a parameter that you won't have in the second method.

Best regards,

Philippe