CSEc secure boot and reset signal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CSEc secure boot and reset signal

跳至解决方案
1,661 次查看
snaku_lee
Contributor IV

Hi,

I have a question about the CSEc secure boot with sequential boot mode.

I want to measure the secure boot time from reset pin release to high, but I find there is no different while secure boot with different BOOT_SIZE?

So I guess when the secure boot is start to boot (i.e., the CSEc is computing the CMAC), the CPU core stay in reset state, and the reset pin also hold in low state, until CMAC compuing finish, am I right ?

Regards,

Snaku

标记 (1)
0 项奖励
回复
1 解答
1,645 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Snaku,

You can find some execution time specs in AN5401.

danielmartynek_0-1629891972636.png

You are right, the reset_b pin is driven low as long as the core is in the reset state.

You can measure the time between a rising edge on the VDD power supply (after POR) and the rising edge on reset_b.

 

Regards,

Daniel

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,646 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Snaku,

You can find some execution time specs in AN5401.

danielmartynek_0-1629891972636.png

You are right, the reset_b pin is driven low as long as the core is in the reset state.

You can measure the time between a rising edge on the VDD power supply (after POR) and the rising edge on reset_b.

 

Regards,

Daniel

0 项奖励
回复
1,627 次查看
snaku_lee
Contributor IV

Hi Daniel,

I got it, thanks for your support.

Snaku

0 项奖励
回复