BusFault: A precise (synchronous) data access error has occurred in S32K312, in RTC initialized

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

BusFault: A precise (synchronous) data access error has occurred in S32K312, in RTC initialized

2,763 次查看
LewisThin
Contributor III

I met a fault when initial RTC using mcal

BusFault: A precise (synchronous) data access error has occurred.
Possible BusFault location: 0x40288004.
HardFault: A fault has been escalated to a hard fault. 

LewisThin_0-1705232821854.png

 

 

If I run the program directly, everything is OK

but when i run the program from boot, the program crashed in line 475, the fault is above.

the chip is S32K312

 

can anybody help?

 

0 项奖励
回复
3 回复数

2,529 次查看
Vaibhav_Kawadkar
Contributor I

Hi @danielmartynek ,

We are working on S32K322.

We are also facing same issue in Clock_Ip_SetRtcRtccClksel_TrustedCall()

What could be the possible reasons of failing?

Vaibhav_Kawadkar_0-1717755989643.png

 

0 项奖励
回复

2,539 次查看
nirmal_masilamani
Contributor V

 I am getting hard Fault while running S32K144W MCAL CAN example.

BusFault: A precise (synchronous) data access error has occurred.
Possible BusFault location: 0x40024000.
HardFault: A fault has been escalated to a hard fault.

0 项奖励
回复

2,732 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @LewisThin,

Is PRTN1_COFB1_CLKEN[REQ34] set?

 

Thank you,

BR, Daniel

0 项奖励
回复