BusFault: A precise (synchronous) data access error has occurred in S32K312, in RTC initialized

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BusFault: A precise (synchronous) data access error has occurred in S32K312, in RTC initialized

2,748 Views
LewisThin
Contributor III

I met a fault when initial RTC using mcal

BusFault: A precise (synchronous) data access error has occurred.
Possible BusFault location: 0x40288004.
HardFault: A fault has been escalated to a hard fault. 

LewisThin_0-1705232821854.png

 

 

If I run the program directly, everything is OK

but when i run the program from boot, the program crashed in line 475, the fault is above.

the chip is S32K312

 

can anybody help?

 

0 Kudos
Reply
3 Replies

2,514 Views
Vaibhav_Kawadkar
Contributor I

Hi @danielmartynek ,

We are working on S32K322.

We are also facing same issue in Clock_Ip_SetRtcRtccClksel_TrustedCall()

What could be the possible reasons of failing?

Vaibhav_Kawadkar_0-1717755989643.png

 

0 Kudos
Reply

2,524 Views
nirmal_masilamani
Contributor V

 I am getting hard Fault while running S32K144W MCAL CAN example.

BusFault: A precise (synchronous) data access error has occurred.
Possible BusFault location: 0x40024000.
HardFault: A fault has been escalated to a hard fault.

0 Kudos
Reply

2,717 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @LewisThin,

Is PRTN1_COFB1_CLKEN[REQ34] set?

 

Thank you,

BR, Daniel

0 Kudos
Reply