BusFault: A precise (synchronous) data access error has occurred in S32K312, in RTC initialized

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BusFault: A precise (synchronous) data access error has occurred in S32K312, in RTC initialized

2,780件の閲覧回数
LewisThin
Contributor III

I met a fault when initial RTC using mcal

BusFault: A precise (synchronous) data access error has occurred.
Possible BusFault location: 0x40288004.
HardFault: A fault has been escalated to a hard fault. 

LewisThin_0-1705232821854.png

 

 

If I run the program directly, everything is OK

but when i run the program from boot, the program crashed in line 475, the fault is above.

the chip is S32K312

 

can anybody help?

 

0 件の賞賛
返信
3 返答(返信)

2,546件の閲覧回数
Vaibhav_Kawadkar
Contributor I

Hi @danielmartynek ,

We are working on S32K322.

We are also facing same issue in Clock_Ip_SetRtcRtccClksel_TrustedCall()

What could be the possible reasons of failing?

Vaibhav_Kawadkar_0-1717755989643.png

 

0 件の賞賛
返信

2,556件の閲覧回数
nirmal_masilamani
Contributor V

 I am getting hard Fault while running S32K144W MCAL CAN example.

BusFault: A precise (synchronous) data access error has occurred.
Possible BusFault location: 0x40024000.
HardFault: A fault has been escalated to a hard fault.

0 件の賞賛
返信

2,749件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @LewisThin,

Is PRTN1_COFB1_CLKEN[REQ34] set?

 

Thank you,

BR, Daniel

0 件の賞賛
返信