BESS_Demo_BmsSL_SAF_V0_8_0 build fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BESS_Demo_BmsSL_SAF_V0_8_0 build fail

Jump to solution
840 Views
starwarrior
Contributor II

Hi experts

I'm using BESS_Demo_BmsSL_SAF_V0_8_0. I have installed all the sdk in the dependencies.txt , imported Reference_Application_1500 ,generated code in mex file ,and modified these macros as follow
#define IPCF_IP_CFG_VENDOR_ID_C 43
#define IPCF_IP_CFG_VENDOR_ID 43

When I want to build the porject , I got many erros as below

error.jpg

Then , I found that there is no file in the folder s32k_saf_1_0_4

error.png

Is there any problem?

Thanks

0 Kudos
Reply
1 Solution
812 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Did you install S32K3_SAF_1.0.4_EVAL_DS_updatesite.zip? (BESS\BESS_2024_06\Safety_Software_Framework_Demo_1_0_4\S32K3_SAF_1.0.4_EVAL_DS_updatesite.zip)

install S32K3_SAF_1.0.4_EVAL_DS_updatesite.png

After the installation is complete, you need to modify the Location:

s32k3x_saf_1_0_4 Location.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
813 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Did you install S32K3_SAF_1.0.4_EVAL_DS_updatesite.zip? (BESS\BESS_2024_06\Safety_Software_Framework_Demo_1_0_4\S32K3_SAF_1.0.4_EVAL_DS_updatesite.zip)

install S32K3_SAF_1.0.4_EVAL_DS_updatesite.png

After the installation is complete, you need to modify the Location:

s32k3x_saf_1_0_4 Location.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
800 Views
starwarrior
Contributor II
Hi Robin
Thanks a lot
It turns out that I didn't change the location of this folder.
Now it's all right
Best Regards
Nick
0 Kudos
Reply