Application note about S32K3 eMIOS/TRMUX/ADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Application note about S32K3 eMIOS/TRMUX/ADC

Jump to solution
9,114 Views
Eli_Wang
Contributor II

Hi,We are helping customer debug ADC/eMIOS of S32K314 and need 32 ADC channels to trigger PWM.  Would you please share application note related with eMIOS/TRMUX/ADC ? 

0 Kudos
Reply
1 Solution
9,099 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Eli_Wang,

Currently, there is only AN13413 ADC Guidelines Spec and Configuration

https://www.nxp.com/docs/en/application-note/AN13413.pdf

which also covers the triggers.

In mid July, there should be motor control demos available with application notes.

 

Regards,

Daniel

 

View solution in original post

0 Kudos
Reply
8 Replies
9,100 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Eli_Wang,

Currently, there is only AN13413 ADC Guidelines Spec and Configuration

https://www.nxp.com/docs/en/application-note/AN13413.pdf

which also covers the triggers.

In mid July, there should be motor control demos available with application notes.

 

Regards,

Daniel

 

0 Kudos
Reply
4,779 Views
StabFlo
Contributor II
Hi,
sadly the link is dead.
BR
Florian
0 Kudos
Reply
4,765 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @StabFlo,

Unfortunately, the AN was temporarily removed from the NXP webpage because of some inconsistencies.

We don't have any target date for the update yet.

 

Regards,

Daniel

0 Kudos
Reply
4,909 Views
MVR
Contributor V

Hello, 

I"m facing "Page Not Found"

Where can I find application note docs about S32K344?

Thanks.

6,198 Views
Kazarian
Contributor III

@danielmartynek  the link does not work, can you please share the new link for this.

0 Kudos
Reply
7,017 Views
Ralphty
Contributor II
0 Kudos
Reply
9,069 Views
Eli_Wang
Contributor II

Thanks, there is another question. The customer found that when the bctu module and emios (Opwmt mode) open the interrupt at the same time, the emios interrupt cannot enter. Is there anything to pay attention to when these two modules open the interrupt at the same time?

0 Kudos
Reply
9,071 Views
Eli_Wang
Contributor II

Ok,thanks for reply. 

0 Kudos
Reply